opensource license

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

opensource license

1,950件の閲覧回数
jhPARKING
Contributor I

capture.PNG

hello

I am using the S32K144 product and opensource provided by nxp.
I am using a tool called Fossid to check open source licenses.
I tested it using this tool, and the result was GNU General Public License v3.0 only in a specific source.
The sources are adap_gpio.c and adap_debug.c.
Do these sources have GNU General Public License v3.0 only or are they freely available?

0 件の賞賛
返信
3 返答(返信)

1,929件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

which SW package is that? It's not mentioned in your description.

Regards,

Lukas

0 件の賞賛
返信

1,925件の閲覧回数
jhPARKING
Contributor I

It is a source automatically generated by S32K Design Studio for ARM.

0 件の賞賛
返信

1,902件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Well, I have S32DS for ARM 2.2 and also older version 2018.R1 but there are no such files.

What is the path? I guess it's some additional installed package.

Regards,

Lukas

0 件の賞賛
返信