network path for s32 design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

network path for s32 design studio

ソリューションへジャンプ
3,618件の閲覧回数
sanjay645
Contributor I

Hello, I want to put the dependent libraries on a network and build the project on my local system.

For example in the image attached, I want to change "HSE_DIR_PATH" from local path of my sytem to a remote path (located on some server like one drive).

It this possible in s32 design studio to provide a network path of library? Please let me know.

0 件の賞賛
返信
1 解決策
3,377件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you need to map the network drive into OS - let's say as a drive N: or what you want - https://support.microsoft.com/en-us/windows/map-a-network-drive-in-windows-29ce55d1-34e3-a7e2-4801-1... 

元の投稿で解決策を見る

3 返答(返信)
3,588件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @sanjay645 , 

 

If the library is accessible by system - there is no problem to use it from network drive. 

 

You would need to add path to library in project properties as shown below: 

Mehul_Patel_NXP_0-1695300231293.png

 

Please let us know if it works or you have any issue.

 

Thank you. Best regards. 

 

- Mehul Patel

0 件の賞賛
返信
3,539件の閲覧回数
sanjay645
Contributor I

My question was how to put a network location on path in eclipse as eclipse takes only local path of my laptop but files I want to put on my server, not on my laptop.

0 件の賞賛
返信
3,378件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

you need to map the network drive into OS - let's say as a drive N: or what you want - https://support.microsoft.com/en-us/windows/map-a-network-drive-in-windows-29ce55d1-34e3-a7e2-4801-1...