network path for s32 design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

network path for s32 design studio

Jump to solution
3,612 Views
sanjay645
Contributor I

Hello, I want to put the dependent libraries on a network and build the project on my local system.

For example in the image attached, I want to change "HSE_DIR_PATH" from local path of my sytem to a remote path (located on some server like one drive).

It this possible in s32 design studio to provide a network path of library? Please let me know.

0 Kudos
Reply
1 Solution
3,371 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you need to map the network drive into OS - let's say as a drive N: or what you want - https://support.microsoft.com/en-us/windows/map-a-network-drive-in-windows-29ce55d1-34e3-a7e2-4801-1... 

View solution in original post

3 Replies
3,582 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @sanjay645 , 

 

If the library is accessible by system - there is no problem to use it from network drive. 

 

You would need to add path to library in project properties as shown below: 

Mehul_Patel_NXP_0-1695300231293.png

 

Please let us know if it works or you have any issue.

 

Thank you. Best regards. 

 

- Mehul Patel

0 Kudos
Reply
3,533 Views
sanjay645
Contributor I

My question was how to put a network location on path in eclipse as eclipse takes only local path of my laptop but files I want to put on my server, not on my laptop.

0 Kudos
Reply
3,372 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you need to map the network drive into OS - let's say as a drive N: or what you want - https://support.microsoft.com/en-us/windows/map-a-network-drive-in-windows-29ce55d1-34e3-a7e2-4801-1...