it can't run FreeRTOS example on S32K312 platform by S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

it can't run FreeRTOS example on S32K312 platform by S32DS

跳至解决方案
3,784 次查看
f-nelson
Contributor IV

Hi NXP:
I tried to run FreeRTOS example on S32K312 platform, but it always be failed at exceptions.c file (HardFault_Handler function) finally,
and it looks like error about configuring the clock dividers that are under MCU control. Could you please tell me how debug this issue? thanks.

Test condition-
S32K312 IC part number:
S32K312NHT0VPAST

installed environment:
1.S32DS IDE:(S32DS.3.4_b201217_win32.x86_64.exe)
2.S32K3 Service Pack:SW32K3_S32DS_3.4.3_D2112.zip
3.S32K3 RTD 2.0.0 package (SW32K3_RTD_4.4_2.0.0_D2203.exe)
4.S32K3 FreeRTOS (SW32K3_FreeRTOS_10_4_6_UOS_2_0_0_DS_updatesite_D2204.zip)

create project method:
1.open IDE
2.File\New\S32DS Project from Example
3.Examples:SW32K3_FreeRTOS 10.4.6 UOS 2.0.0 D2204 Example projects\FreeRTOS_Toggle_Led_Example_S32K312

0 项奖励
回复
1 解答
3,595 次查看
f-nelson
Contributor IV
Hi Robin:
thanks for your helping.
updated status~~we found issue about HSE fw,because I took project board which including HSE fw inside MCU, so example code can't run. I changed new board and no HSE fw in MCU, it can works without issue.

在原帖中查看解决方案

0 项奖励
回复
10 回复数
3,778 次查看
f-nelson
Contributor IV

attached screenshot

0 项奖励
回复
3,747 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Have you modified FreeRTOS_Toggle_Led_Example_S32K312? I tested it on S32K312EVB-Q172 without HSE installed and there was no problem.
It is not recommended to use such an old version. The new version of RTD fixes many bugs. I noticed that the clock configuration in Clocks Tool does not match the "Table 152. Option B - Reduced Speed ​​mode (CORE_CLK @ 120 MHz)" of S32K3XXRM. This example incorrectly sets PLL_PHI0_CLK to 160MHz.

If there is no specific reason, we recommend using a newer version of the software.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
3,702 次查看
f-nelson
Contributor IV
Hi Robin:
thanks for your replying.
In actually,I had modified MCU package from 172pin to 100pin for current project.
I also compared hardware of oscillator component between S32K312EVB-Q172 and current project are the same 16Mhz,
but I am not clear why MCU code always be failed at clock part.Does it have any ideas for checking?

Just now, I tried to modify PLL_PHI0_CLK speed from 160Mhz to 120Mhz,unfortunately the result is the same.

Could you please provide me about recommanding RTD driver version full name and download location? I can try again.
0 项奖励
回复
3,691 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Please find a new version FreeRTOS by click S32K3 Reference Software -> Automotive SW - S32K3 - FreeRTOS

SW32K3 FreeRTOS 11.1.0 version 5.0.0 Code Drop is based on S32K3 RTD 5.0.0 (recommended) 

SW32K3 FreeRTOS 10.6.0 version 4.0.0 is based on S32K3 RTD 4.0.0

If the external circuit is the same, just switching from 172pin to 100pin should not cause this error.
In addition to the 16MHz crystal, is the 32.768kHz slow crystal also connected?

0 项奖励
回复
3,683 次查看
f-nelson
Contributor IV
Hi Robin:


1.SW32K3 FreeRTOS 11.1.0 version 5.0.0 Code Drop is based on S32K3 RTD 5.0.0 (recommended)
=>I checked list of S32K3 Reference Software, but it didn't list "S32K RTD 5.0.0" item for downloading.
download website:https://nxp.flexnetoperations.com/control/frse/product?entitlementId=150312151&lineNum=1&authContact...

2.SW32K3 FreeRTOS 10.6.0 version 4.0.0 is based on S32K3 RTD 4.0.0 <=(AUTO-SW-PACKAGE-MANAGER)
=>I used AUTO-SW-PACKAGE-MANAGER as screenshot for downloading FreeRTOS 4.0.0 and Real-Time Drivers 4.0.0, but
it is pending until now.

3.hardware crystal comparison
S32K312EVB-Q172 schematic:only one 16Mhz crystal
EXTAL=pin23
XTAL=pin25

current project
S32K312-100pin:only one 16Mhz crystal
EXTAL=pin15
XTAL=pin17
we don't have other crystal of 32.768kHz on board now.
0 项奖励
回复
3,617 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Which software did you apply for in the Automotive Software Package Manager? It will recommend the complete dependent software packages.
Have you filled in the detailed information as prompted? In addition, please click Export Control for more information.
If you want to install SW32K3 FreeRTOS 10.6.0 version 4.0.0 based on S32K3 RTD 4.0.0, please try to install S32K3 RTD 4.0.0 by refer to: HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5
Then install SW32K3 FreeRTOS 10.6.0 version 4.0.0 offline.

I haven't written about how to offline install S32K3 RTD 5.0.0, but the method is the same. Just refer to the Release Note of RTD:
1. Install S32Design Studio 3.5: S32DS.3.5_b220726_win32.x86_64.exe
2. Install Update 13 for S32DS: SW32_S32DS_3.5.13_D2407.zip
3. Install development package for S32K3XX: SW32K3_S32DS_3.5.13_D2407
4. Install development package for S32K396: SW32K39x_S32DS_3.5.13_D2407.zip
5. Install development package for S32M276: SW32M2_S32DS_3.5.13_D2407
6. Install updatesite for this release: SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410_DesignStudio_updatesite.
zip

A3: Change the crystal pins in Pins Tool. Disable the 32.768kHz SXOSC:

Disable SXOSC_CLK.SXOSC_CLK.jpg

0 项奖励
回复
3,639 次查看
f-nelson
Contributor IV
Hi Robin:
I found S32K3 RTD 5.0.0(SW32K3_S32M27x_RTD_R21-11_5.0.0_D2410.exe), is it correct? thanks
0 项奖励
回复
3,596 次查看
f-nelson
Contributor IV
Hi Robin:
thanks for your helping.
updated status~~we found issue about HSE fw,because I took project board which including HSE fw inside MCU, so example code can't run. I changed new board and no HSE fw in MCU, it can works without issue.
0 项奖励
回复
3,586 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

If HSE FW is installed and S32K3 RTD 2.0.x is used, it is recommended to disable FIRC. Refer to this discussion: S32K3_HSE_BUG_RTD2.0.x

0 项奖励
回复
3,582 次查看
f-nelson
Contributor IV
thanks again~~it's useful.
0 项奖励
回复