installation manager not include touchpoint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

installation manager not include touchpoint

ソリューションへジャンプ
348件の閲覧回数
yangcao1234
Contributor II

S32DS 2.2 install S32DS_ARM_v2018.R1_UP6 reminder installation manager not include touchpoint.

Could you provide me some fixed package or solution? Thanks!

0 件の賞賛
返信
1 解決策
337件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please do not install S32DS_ARM_v2018.R1_UP6 in S32 Design Studio for ARM Version 2.2.
Do you want to install SDK S32K1xx RTM SR 3.0.3 (Patch for SDK S32K1xx RTM 3.0.0), if so please install S32 Design Studio for ARM 2.2 - Update 1 ?

If you expect to use the SDK in S32 Design Studio for Arm 2018.R1 - Update 6, then you should install S32 Design Studio for ARM 2018.R1 (Windows/Linux)

Best Regards,
Robin

元の投稿で解決策を見る

2 返答(返信)
338件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please do not install S32DS_ARM_v2018.R1_UP6 in S32 Design Studio for ARM Version 2.2.
Do you want to install SDK S32K1xx RTM SR 3.0.3 (Patch for SDK S32K1xx RTM 3.0.0), if so please install S32 Design Studio for ARM 2.2 - Update 1 ?

If you expect to use the SDK in S32 Design Studio for Arm 2018.R1 - Update 6, then you should install S32 Design Studio for ARM 2018.R1 (Windows/Linux)

Best Regards,
Robin

331件の閲覧回数
yangcao1234
Contributor II
Thanks.
0 件の賞賛
返信