install free RTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

install free RTOS

Jump to solution
3,169 Views
monk_65
Contributor III

 

hi ,

i installed version RTS 3.00 for S32K344

and i have a failure when i want install package FREERTOS 3.00

install_3_00.PNG

 

install_freertos.PNG

 

0 Kudos
Reply
1 Solution
3,112 Views
monk_65
Contributor III

thank you for the reply

View solution in original post

0 Kudos
Reply
2 Replies
3,126 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

I see that you installed S32K3 RTD 3.0.0, so it is recommended to install 10.5.1_3.1.0 SW32K3_FreeRTOS_10.5.1_3.1.0_D2304 offline. Refer to the offline installation method mentioned in HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5.

FreeRTOS S32K3 RTD 3.0.0.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,113 Views
monk_65
Contributor III

thank you for the reply

0 Kudos
Reply