how it do for S32K148 bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how it do for S32K148 bootloader

4,984 Views
2006070224wmy
Contributor I

Hi,

I want to design a bootloader for S32K148, but I don't want to power off to upgrate the app.

I want to upgrate the app when old app is running,how do I do?

0 Kudos
Reply
6 Replies

4,017 Views
hkaracali
Contributor II

Hello,

I have downloaded https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip and it works successfully. There is one issue. Bootloader interface sends SREC line data at least 50ms intervals. It is huge duration for big SREC files. For instance, sending 200KB SREC file takes more than 4 min. Can you share source code of Bootloader Interface or is there faster version of it?

Best regards. 

0 Kudos
Reply

4,536 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

I'm afraid there is no possibility to run the bootloader and the user application at the same time.

However, the S32Kxx bootloader AN12218 can be useful, but there is needed to jump from bootloader to the application.

https://www.nxp.com/docs/en/application-note/AN12218.pdf 

SW:

https://www.nxp.com/docs/en/application-note-software/AN12218SW.zip 

Best Regards,

Diana

0 Kudos
Reply

3,812 Views
christofhaiding
Contributor IV

Hi Diana!

I downloaded the AN12218SW zip file.

But I cannot open any of the Project included in this download with my S32DS.
Any tips to do this.

Regards

Christof

0 Kudos
Reply

4,536 Views
2006070224wmy
Contributor I

Hi,Diana,

I have another problem.In the project,when I install Serial_Bootloader_Interface.jar ,I have a probem.

1.png

 Do you have 64-bit PC software?

Best Regards,

Carol

0 Kudos
Reply

4,536 Views
ianchu
Contributor I

The solution to your error message is double quotes around the head and tail, which looks like

"C:\program files\java\jre7\bin\javaw.exe"

0 Kudos
Reply

4,536 Views
2006070224wmy
Contributor I

Hi,Diana,

Thank you for your reply. I have read the document and the project.

But it need power cuts to upgrade the app without timeout.

pastedImage_1.png

And I need to upgrade the app without running out of the power.

0 Kudos
Reply