fs2322b

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,865件の閲覧回数
zq1
Contributor III

i am building a project with a sbc called fs2322b ,but there is no examples can be helpful ,what i can find is only below ,but it is not useful for me,

企业微信截图_17027186697391.png

 so is there some other example that can be provided to me ,thank you .

then, when i read the datasheet of fs2322,there are some verbs i can not understand ,like below:

zq1_0-1702718981973.png

what's meaning of otp fuse,i need your help ,as soon as possible,

0 件の賞賛
返信
1 解決策
1,830件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

I am not aware of any other FS23 software drivers and code examples.

OTP fuse means that the value of these bits depends on their OTP configuration. For example, the LIN_EN bit will be 0 (= LIN disabled) if the corresponding LIN_EN_OTP bit is 0. Similarly, the LIN_EN bit will be 1 (= LIN enabled) if the LIN_EN_OTP bit is 1.

In case of the FS2322B, LIN_EN_OTP = 0 (= LIN disabled) and consequently LIN_EN is also 0.

Capture.JPG

BR, Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,831件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello,

I am not aware of any other FS23 software drivers and code examples.

OTP fuse means that the value of these bits depends on their OTP configuration. For example, the LIN_EN bit will be 0 (= LIN disabled) if the corresponding LIN_EN_OTP bit is 0. Similarly, the LIN_EN bit will be 1 (= LIN enabled) if the LIN_EN_OTP bit is 1.

In case of the FS2322B, LIN_EN_OTP = 0 (= LIN disabled) and consequently LIN_EN is also 0.

Capture.JPG

BR, Tomas

0 件の賞賛
返信