freertos+s32k

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,466件の閲覧回数
kalajiao
Contributor II

I joined the freertos on s32k board, and then create a simple task in it as well as an interrupt the callback function, want to test the recovery of the suspension of tasks and inside the interrupt, but there was a problem, is at the time of task, stuck in a function out, don't know why, as the chart

QQ截图20210722140257.png

This is my overall callback function

中断回复任务出不来的地方.png

This is where the loop goes all the way up here

0 件の賞賛
返信
1 解決策
3,460件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the answer in: About the button
Please try to clear interrupt flag in callback(buttonisr).

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
1 返信
3,461件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Please check the answer in: About the button
Please try to clear interrupt flag in callback(buttonisr).

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

タグ(1)
0 件の賞賛
返信