emios pwm configuration for 40% duty cycle of 1 second

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

emios pwm configuration for 40% duty cycle of 1 second

3,458 Views
semiconductor_user
Contributor III

MCU : s32k324 

PIN : PTE10 (LED)

Inatnace : Emios0

Emios CH number : 20

Clock freq = 160 MHZ

i'm triying to configuration eMISO_PWM for 40% duty cycle of 1 second for that i want to know  calculation formula and value of counter(tick), prescaler. base on above mention paramter.

and also shared Screenshot of configuration and code

 

0 Kudos
Reply
3 Replies

3,422 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @semiconductor_user 

Check the following thread, it has information related to the topic that may be useful to you.

s32k312 emios pwm period

 

BR, VaneB

0 Kudos
Reply

3,416 Views
semiconductor_user
Contributor III

hello @VaneB 

thank you for resopnce 

but i'm still confuse  

my requirement is i want to generate 40% duty cycle of 1 second period. base on this equation PWM frequency = CORE_CLK / global prescaler / internal prescaler / (B1+1).

for that we below mention parameters 

Emios Mcl (module)

1. Clock Divider value (global prescaler)

2. default period

3. Master bus prescaler

4. Master bus Alternate prescaler

Emios Pwm (module)

mode : EMIOS_PWM_IP_MODE_OPWMB

Clock prescaler

Clock prescaler Alternate

Duty cycle [tick]

period [tick]

please share configuration value for this parameter.

 

0 Kudos
Reply

3,409 Views
VaneB
NXP TechSupport
NXP TechSupport

hi @semiconductor_user 

As you said, the EMIOS module setting in ConfigTools are named as Clock_Divider Value, Master_Bus Prescaler, and Master BusAlternate Prescaler. How to know their relationship and their usage according to the formula provided in the thread shared above?

PWM frequency = CORE_CLK / Clock Divider Value / Master Bus Prescaler / period [ticks]

With this information, if we want a PWM of 1KHz and the clock frequency of our eMIOS is 48Mhz and we define the Clock Divider Value and the Master Bus Prescaler equal to 1, with this we would only need one parameter to obtain our 1KHz signal, which is the period [tick] which we can obtain by solving the formula given above:

period [tick] = CORE_CLK/1KHz, giving 48,000.

To set the Duty cycle [tick] of this signal, we assume a duty cycle of 100% is equal to the period [tick](48000 ticks), so a duty cycle of 40% will be equal to a (period [tick]*40)/100 = 19,200 ticks approx.

Additionally, with a 16-bit timer the maximum number of tick (ticksmax) is (2^16 − 1) = 65,535 ticks. If we configure the eMIOS with a fClock of 48MHz (fClock  = CORE_CLK / Clock Divider Value / Master Bus Prescaler) we have a tick every 1/(fClock ) = 1/48MHz = 0.02083μs approx (it depends on your configurations).

0 Kudos
Reply