eMIOS Channel Internal Timebase Interference

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMIOS Channel Internal Timebase Interference

2,060件の閲覧回数
vusal
Contributor III

Hello,

Does the internal counter have an effect outside of its own channel? For example, if I have two channels (one input and one output) running on their own internal timebase will they interfere with each other? In this diagram it seems like the internal counter feeds back to the Counter bus.

Thanks!
Vusal

vusal_0-1727472777709.pngvusal_0-1727472777709.png

 

0 件の賞賛
返信
4 返答(返信)

2,015件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@vusal

Some channels have internal counters, which can be output as Couner_bus_A, Couner_bus_B, Couner_bus_C, Couner_bus_D, Couner_bus_F.

Senlent_0-1727576644885.pngSenlent_0-1727576644885.png

 

1,992件の閲覧回数
vusal
Contributor III

Hi @Senlent ,

Thank you for your message!

Any thoughts on when reading A and B in the IPM mode, FLAG bit doesn't get set and instead I have the OVFL bit?

Thanks!
Vusal


0 件の賞賛
返信

1,974件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@vusal

please read the S32K3'RM ,the chapter 63.5.3.11 Input Period Measurement (IPM) Mode for detail.

Senlent_0-1727747508389.pngSenlent_0-1727747508389.png

 

0 件の賞賛
返信

2,054件の閲覧回数
vusal
Contributor III

BTW, this is for s32K3xx.

0 件の賞賛
返信