eMIOS Channel Internal Timebase Interference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMIOS Channel Internal Timebase Interference

2,076 Views
vusal
Contributor III

Hello,

Does the internal counter have an effect outside of its own channel? For example, if I have two channels (one input and one output) running on their own internal timebase will they interfere with each other? In this diagram it seems like the internal counter feeds back to the Counter bus.

Thanks!
Vusal

vusal_0-1727472777709.pngvusal_0-1727472777709.png

 

0 Kudos
Reply
4 Replies

2,031 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@vusal

Some channels have internal counters, which can be output as Couner_bus_A, Couner_bus_B, Couner_bus_C, Couner_bus_D, Couner_bus_F.

Senlent_0-1727576644885.pngSenlent_0-1727576644885.png

 

2,008 Views
vusal
Contributor III

Hi @Senlent ,

Thank you for your message!

Any thoughts on when reading A and B in the IPM mode, FLAG bit doesn't get set and instead I have the OVFL bit?

Thanks!
Vusal


0 Kudos
Reply

1,990 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@vusal

please read the S32K3'RM ,the chapter 63.5.3.11 Input Period Measurement (IPM) Mode for detail.

Senlent_0-1727747508389.pngSenlent_0-1727747508389.png

 

0 Kudos
Reply

2,070 Views
vusal
Contributor III

BTW, this is for s32K3xx.

0 Kudos
Reply