Have you tried adding the build path to the specific configuration you are using?
"Right click -> Build path -> Add to -> Release_XXX"
There are no specific guides for includes and such for S32DS, but since it is based in eclipse, you can use the same guides for normal eclipse:
Hope this helps.
Are you using a repository with the project? The question mark means the code is not yet added and committed to your repository. This is normal and would disappear as soon as you commit your code to git.
This is eclipse functionality. It should not affect building, as long as the folders are included in the project's properties.
Best regards,
Julián
hi @Julián_AragónM, my project is building in debug flash but give file not detected in the release mode i checked the paths and symbol and the includes both are same but its not able to detect the files, i had attached the project can you check why is it giving this error
Have you tried adding the build path to the specific configuration you are using?
"Right click -> Build path -> Add to -> Release_XXX"
There are no specific guides for includes and such for S32DS, but since it is based in eclipse, you can use the same guides for normal eclipse:
Hope this helps.
hi @Julián_AragónM i had tried this before this too isn't working , i have to check the .h calls maybe if its called in the loop inside different module
thank you
hi @Julián_AragónM thank you for the symbol definitions , is there any document as how to add directory , header file and source file to the project as i tried to add it in many ways like a source folder and as normal folder.