daisy chain problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

daisy chain problem

Jump to solution
4,233 Views
Shreyas_Bhat_Karkala
Contributor III

Hi there,

We are currently attempting to initialize RDBMSCTBNU by leveraging the example code provided for HVBMS (HvBms400_775_722_TPL_Bring_Up) using the TPL 665a variant. The goal is to read measurement registers from the 775a. However, we are encountering an issue related to SL extraction.

The problem arises when the start measurement write operation is broadcasted to all devices simultaneously. In this scenario, SL extraction fails. Conversely, if the start measurement register is written individually for each device, the measurement values for all four AFEs become visible.

For reference, I have attached the CMU.c code with and without the implemented changes.

Best regards.

 

Tags (2)
0 Kudos
Reply
1 Solution
4,041 Views
Shreyas_Bhat_Karkala
Contributor III

The evaluation Board came with one 12 V power supply so we used a 5V power supply which came with the other evaluation kit for the AFEs , so this issue showed up , it was showing UV and was giving the Safety library(SL) issue.   

View solution in original post

Tags (2)
0 Kudos
Reply
3 Replies
4,204 Views
Shreyas_Bhat_Karkala
Contributor III

I had attached the files in the previous post but it was not present so i am re attaching the code .
BR

0 Kudos
Reply
4,042 Views
Shreyas_Bhat_Karkala
Contributor III

The evaluation Board came with one 12 V power supply so we used a 5V power supply which came with the other evaluation kit for the AFEs , so this issue showed up , it was showing UV and was giving the Safety library(SL) issue.   

Tags (2)
0 Kudos
Reply
4,162 Views
RafaR
NXP Employee
NXP Employee

Okay

Thanks for your interest in NXP products.

I will contact you soon, I need to check more details about the problem.

 

Have a great day and best of luck.

0 Kudos
Reply