compilation error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

compilation error

1,187 Views
aaz1234
Contributor II

I am trying to build an example project on s32 design studio version 3.6.4 and getting this error

 

Screenshot 2026-03-18 091017.png

Tags (1)
0 Kudos
Reply
3 Replies

1,161 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @aaz1234 

Please refer to the following threads where a similar error has been discussed:

Also, could you please provide your installation details, the example you are working with, and the steps you followed? That way, I can try to reproduce the issue on my side.

 

BR, VaneB

0 Kudos
Reply

1,156 Views
aaz1234
Contributor II

Thanks for the reply. I am working on Dio example for s32k3 board. I have downloaded the RTD drivers for those applications. 

 

i was able to solve the other problems but now i am having these errors

 

Screenshot 2026-03-18 215716.png

Tags (1)
0 Kudos
Reply

1,140 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @aaz1234 

Which RTD version are you currently working with?

How was the example project imported into your workspace? Did you use the “S32DS Project from Example” option? Did you generate the missing configuration files by updating the code through ConfigTools?

Also, the error messages refer to include paths such as header, include, and startup/include. Please verify that these paths actually exist in your installation, for example:

C:\NXP\S32DS.3.6.4\S32DS\software\PlatformSDK_S32K3\RTD\BaseNXP_TS_T40D34M60I0R0\header

0 Kudos
Reply