check stack & heap size during debug in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

check stack & heap size during debug in S32DS

ソリューションへジャンプ
3,397件の閲覧回数
skseofh
Contributor II

Hi

I'm using S32144 and S32DS.

 

During Debugging, is there any way to check stack & heap size?

 

If there is, please let me know!

Thanks

0 件の賞賛
返信
1 解決策
3,386件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

these discussions could be helpful:

https://community.nxp.com/t5/S32-Design-Studio/How-to-check-CPU-Usage/m-p/743398

https://community.nxp.com/t5/S32K/Failure-reaction-in-case-of-Stack-overflow-or-underflow-S32K1/m-p/...

https://community.nxp.com/t5/S32K/Example-of-DWT-for-stack-usage-monitoring-on-S32K1xx/td-p/1160990

In addition, I like this simple high water mark method: fill whole stack by some pattern like 0xAA (for example by debugger) and then run the code. Examine as many program paths as possible and then check the stack – you will see which part of the stack has been rewritten and you can adjust the size accordingly.

Regards,

Lukas

 

元の投稿で解決策を見る

1 返信
3,387件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

these discussions could be helpful:

https://community.nxp.com/t5/S32-Design-Studio/How-to-check-CPU-Usage/m-p/743398

https://community.nxp.com/t5/S32K/Failure-reaction-in-case-of-Stack-overflow-or-underflow-S32K1/m-p/...

https://community.nxp.com/t5/S32K/Example-of-DWT-for-stack-usage-monitoring-on-S32K1xx/td-p/1160990

In addition, I like this simple high water mark method: fill whole stack by some pattern like 0xAA (for example by debugger) and then run the code. Examine as many program paths as possible and then check the stack – you will see which part of the stack has been rewritten and you can adjust the size accordingly.

Regards,

Lukas