cannot see printf output on semihosting using jlink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot see printf output on semihosting using jlink

1,997件の閲覧回数
sanjay645
Contributor I

Hello, I am using jlink with s32k3 on s32 design studio. When I create a new project using "new lib" and i use printf, i can see printf output on my debug console, but when use an existing project, i use printf then there is no output of printf on debug console. I searched on internet and came to know that I have to enable "newlib debug console" by clicking on project settings under Target processor->Library support as shown in the figured, but after even enabling the library I am not able to see printf output :

I also compared project settings of my older project where printf output is no displaying on console with the new project i created in which prints are visible, both settings are same but i am not able to see prints on my older project. Please help me what can go wrong?

sanjay645_0-1697004241704.png

 

0 件の賞賛
返信
1 返信

1,922件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you enabled the semihosting console in debug configurations? 

jiri_kral_0-1702049284359.png

 

0 件の賞賛
返信