cannot see printf output on semihosting using jlink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot see printf output on semihosting using jlink

2,030 Views
sanjay645
Contributor I

Hello, I am using jlink with s32k3 on s32 design studio. When I create a new project using "new lib" and i use printf, i can see printf output on my debug console, but when use an existing project, i use printf then there is no output of printf on debug console. I searched on internet and came to know that I have to enable "newlib debug console" by clicking on project settings under Target processor->Library support as shown in the figured, but after even enabling the library I am not able to see printf output :

I also compared project settings of my older project where printf output is no displaying on console with the new project i created in which prints are visible, both settings are same but i am not able to see prints on my older project. Please help me what can go wrong?

sanjay645_0-1697004241704.png

 

0 Kudos
Reply
1 Reply

1,955 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you enabled the semihosting console in debug configurations? 

jiri_kral_0-1702049284359.png

 

0 Kudos
Reply