/bin/sh: gcc: command not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

/bin/sh: gcc: command not found

Jump to solution
11,819 Views
phidiawang
Contributor III

Hi:

   I test S/W of MTRDEVKSPNK144_S32DS in S32DS 2018.R1.  then Error occurred while compiling .

新建位图图像 (2).jpg

Please help.

 

Thanks.

Tags (1)
1 Solution
10,497 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this project is for S32DS for ARM v1.3 and SDK v1.0.0 - please check release notes: 

The Development Kit application was built and tested using the following IDE and SDK:
=============================================================================
- S32 Design Studio (S32DS) for ARM v1.3
- S32 Software Development Kit (SDK) v1.0.0

Jiri

View solution in original post

4 Replies
10,498 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this project is for S32DS for ARM v1.3 and SDK v1.0.0 - please check release notes: 

The Development Kit application was built and tested using the following IDE and SDK:
=============================================================================
- S32 Design Studio (S32DS) for ARM v1.3
- S32 Software Development Kit (SDK) v1.0.0

Jiri

10,497 Views
gaoying
Contributor I
    0 Kudos
    Reply
    10,497 Views
    phidiawang
    Contributor III

    HI,Jiri

       thanks ,I solved this problem。S32 Design Studio (S32DS) for ARM v1.3 is right.

    0 Kudos
    Reply
    10,497 Views
    gaoying
    Contributor I

    请问是否您的问题是怎么解决的?我以前的项目也是v1.3编译的,下载了官网的v2.2版本之后,编译报同样的错误。

    Could you tell me how your problem was solved?My project was also compiled by v1.3. After downloading the v2.2 version of the official website, the compilation reported the same error.

    0 Kudos
    Reply