adc sdk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adc sdk

1,757 Views
siiv
Contributor I

i want a simple example to read adc values in s32k144 evb using driver apis 

 

0 Kudos
Reply
2 Replies

1,698 Views
siiv
Contributor I

i atteched my file below can you tell me the whre i did a mistake in that one.i didnt get the adcvalue(variable name)

0 Kudos
Reply

1,746 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @siiv 

The SDK includes four examples of ADC:

  • ADC Low Power
  • ADC Hardware Trigger
  • ADC PAL example
  • ADC Software Trigger

Also, there are this two examples that you could use as a reference:

Example S32K144 PDB ADC trigger DMA ISR S32DS

Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1

If you do not need to use the SDK, we also have an ADC example in the S32K1xx Series Cookbook and the S32K1xx ADC guidelines, specs, and configuration.

 

B.R.

VaneB

0 Kudos
Reply