adc sdk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adc sdk

1,760件の閲覧回数
siiv
Contributor I

i want a simple example to read adc values in s32k144 evb using driver apis 

 

0 件の賞賛
返信
2 返答(返信)

1,701件の閲覧回数
siiv
Contributor I

i atteched my file below can you tell me the whre i did a mistake in that one.i didnt get the adcvalue(variable name)

0 件の賞賛
返信

1,749件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @siiv 

The SDK includes four examples of ADC:

  • ADC Low Power
  • ADC Hardware Trigger
  • ADC PAL example
  • ADC Software Trigger

Also, there are this two examples that you could use as a reference:

Example S32K144 PDB ADC trigger DMA ISR S32DS

Example S32K144 PDB ADC DMA S32DS.ARM.2018.R1

If you do not need to use the SDK, we also have an ADC example in the S32K1xx Series Cookbook and the S32K1xx ADC guidelines, specs, and configuration.

 

B.R.

VaneB

0 件の賞賛
返信