accessing pin getting error when i used code configure for s32k144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

accessing pin getting error when i used code configure for s32k144

11,684 Views
ash123456789
Contributor III

I am using internal clock oscillator while doing following program and it get stuck at initaillising pins  i dont know why 

#include "sdk_project_config.h"

void delay(volatile uint32_t count) {
while (count--);
}

int main(void) {
/* Initialize Clock System */
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);

PINS_DRV_Init(1,g_pin_mux_InitConfigArr0);


PINS_DRV_WritePin(led_PORT, led_pin,1U);

return 0;
}

0 Kudos
Reply
12 Replies

11,642 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ash123456789,

Could you share either your project or your configuration & config array for the pin mux? It should look something like this:

pin_settings_config_t g_pin_mux_InitConfigArr0[NUM_OF_CONFIGURED_PINS0] = {
    {
        .base            = PORTC,
        .pinPortIdx      = 0U,
        .pullConfig      = PORT_INTERNAL_PULL_NOT_ENABLED,
        .driveSelect     = PORT_LOW_DRIVE_STRENGTH,
        .passiveFilter   = false,
        .mux             = PORT_MUX_AS_GPIO,
        .pinLock         = false,
        .intConfig       = PORT_DMA_INT_DISABLED,
        .clearIntFlag    = false,
        .gpioBase        = PTC,
        .direction       = GPIO_OUTPUT_DIRECTION,
        .digitalFilter   = false,
        .initValue       = 0U,
    },
    {
        .base            = PORTC,
        .pinPortIdx      = 1U,
        .pullConfig      = PORT_INTERNAL_PULL_NOT_ENABLED,
        .driveSelect     = PORT_LOW_DRIVE_STRENGTH,
        .passiveFilter   = false,
        .mux             = PORT_MUX_AS_GPIO,
        .pinLock         = false,
        .intConfig       = PORT_DMA_INT_DISABLED,
        .clearIntFlag    = false,
        .gpioBase        = PTC,
        .direction       = GPIO_OUTPUT_DIRECTION,
        .digitalFilter   = false,
        .initValue       = 0U,
    },
    {
        .base            = PORTD,
        .pinPortIdx      = 15U,
        .pullConfig      = PORT_INTERNAL_PULL_NOT_ENABLED,
        .driveSelect     = PORT_LOW_DRIVE_STRENGTH,
        .passiveFilter   = false,
        .mux             = PORT_MUX_AS_GPIO,
        .pinLock         = false,
        .intConfig       = PORT_DMA_INT_DISABLED,
        .clearIntFlag    = false,
        .gpioBase        = PTD,
        .direction       = GPIO_OUTPUT_DIRECTION,
        .digitalFilter   = false,
        .initValue       = 0U,
    },
    {
        .base            = PORTD,
        .pinPortIdx      = 16U,
        .pullConfig      = PORT_INTERNAL_PULL_NOT_ENABLED,
        .driveSelect     = PORT_LOW_DRIVE_STRENGTH,
        .passiveFilter   = false,
        .mux             = PORT_MUX_AS_GPIO,
        .pinLock         = false,
        .intConfig       = PORT_DMA_INT_DISABLED,
        .clearIntFlag    = false,
        .gpioBase        = PTD,
        .direction       = GPIO_OUTPUT_DIRECTION,
        .digitalFilter   = false,
        .initValue       = 0U,
    },
  };

You can also refer to the existing examples for the s32k144 (such as hello_world_s32k144) which configures two LEDs (LED0 & LED1) and toggles them in the main function.

Best regards,
Julián

0 Kudos
Reply

11,629 Views
ash123456789
Contributor III

at pins drv init program counter directly  going to  default isr and showing some issue but fr bare led blink its working

0 Kudos
Reply

11,606 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ash123456789,

It seems you are only initializing one pin in your function; you can replace the "1" with the generated config as "NUM_OF_CONFIGURED_PINS0".

Also, you are using the CLOCK_SYS_Init function instead of CLOCK_DRV_Init. Clock DRV init configures the clocks for the used ports. Please test the example first then try to implement your new project on top of it:

hello_world_s32k144:

int main(void)
{
  status_t error;
  /* Configure clocks for PORT */
  error = CLOCK_DRV_Init(&clockMan1_InitConfig0);
  DEV_ASSERT(error == STATUS_SUCCESS);
  /* Set pins as GPIO */
  error = PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
  DEV_ASSERT(error == STATUS_SUCCESS);

  /* Set Output value LED0 & LED1 */
  PINS_DRV_SetPins(LED0_PORT, 1 << LED0_PIN);
  PINS_DRV_ClearPins(LED1_PORT, 1 << LED1_PIN);

  for (;;)
  {
      /* Insert a small delay to make the blinking visible */
      delay(720000);

      /* Toggle output value LED0 & LED1 */
      PINS_DRV_TogglePins(LED0_PORT, 1 << LED0_PIN);
      PINS_DRV_TogglePins(LED1_PORT, 1 << LED1_PIN);
  }
}

Best regards,
Julián

 

0 Kudos
Reply

11,575 Views
ash123456789
Contributor III

like you said i tried and see program counter is going in defaault isr 

0 Kudos
Reply

11,557 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ash123456789,

As I've said in my previous replies, please test the included example first, as it may be easier to compare the working project. I've attached it here to my reply.

Best regards,
Julián

0 Kudos
Reply

11,546 Views
ash123456789
Contributor III

I run your example on my board and there is issue in initialize clock it is getting stuck or waiting to sock clk to start but it has some issue 

0 Kudos
Reply

11,524 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ash123456789,

Are you using a custom board? If so, this issue may be caused by hardware design. You can follow the Hardware Design Guidelines for S32K1.

If you are using an EVB, please make sure the jumpers are in the right configuration.

Best regards,
Julián

0 Kudos
Reply

11,500 Views
ash123456789
Contributor III
Hi, Julián_AragónM
On my custom board we r not connected in external crystal for clock, i am using internal FIRC OR LIRC as clock source do you have any reference related to this or any example code how to use ?
0 Kudos
Reply

11,479 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ash123456789,

If you wish to change your clock configuration, please refer to the following community post which already explained this: S32k144 clock source change - NXP Community.

Best regards,
Julián.

0 Kudos
Reply

11,345 Views
ash123456789
Contributor III
give me one example which can run on internal clock with code configurator if possible share one example zip with only internal clk and any peripheral driver configure please
0 Kudos
Reply

11,299 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @ash123456789,

There are many examples in the SDK which use a different clock source. For example, the "power_mode_switch_s32k144" uses SIRC:

Julin_AragnM_0-1735926967168.pngJulin_AragnM_1-1735926971492.png

Best regards,
Julián

0 Kudos
Reply

11,664 Views
ash123456789
Contributor III
its woring on bare metal by register configure but i am only getting issue at code configator
0 Kudos
Reply