Why are all registers 0xFFFFFFFF in LPIT0 module?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why are all registers 0xFFFFFFFF in LPIT0 module?

1,263 Views
Ashlie
Contributor III

Hello,

When I try to  use LPIT0 module as a periodic timer, it doesn't work at all. And then, I find that all the registers except VERID are 0xFFFFFFFF. Why?

943552732_0-1679970052539.png

943552732_1-1679970075735.png

I would really appreciate it if anyone could give me a answer.

Best regards,

Ashlie

 

 

0 Kudos
Reply
3 Replies

1,251 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@943552732

so you're using S32K14x series MCU right?

you can take a look at the demo in S32 DS,the name is "lpit_periodic_interrupt_s32k142"

0 Kudos
Reply

1,247 Views
Ashlie
Contributor III

Sorry, I just find that it's the compiler display issue. The lpit0 configuration is ok. It never comes into the interrupt I want but runs into a defaultISR when I configure a interrupt enable in EBTresos as the picutre:

943552732_0-1679985876652.png

943552732_1-1679985897842.png

Maybe it's because I didn't add the interrupt handler into vector table.But what should I do for the next step?

 

Tags (2)
0 Kudos
Reply

1,231 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ashlie

Sorry, I am not familiar with EB tools,you can create a new topic on this forum.

next time,please remember to fill in the complete part number and add some key words in your topic,such as MCAL,EB ,etc, so that your issues will be resloved much faster.

0 Kudos
Reply