Why LCU is used for PWM?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why LCU is used for PWM?

跳至解决方案
2,144 次查看
anakha
Contributor III

Do and why we need to route eMios PWM to LCU through TRGMUX?

What advantages does LCU provides?

 

I am using RTD (3.0.0) with non-autosar.

标记 (4)
0 项奖励
回复
1 解答
2,120 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @anakha 

Do and why we need to route eMios PWM to LCU through TRGMUX? The Enhanced Modular IO Subsystem (eMIOS), Logic Control Unit (LCU), Trigger MUX (TRGMUX), Body Cross-triggering Unit (BCTU) and Analogue-to-Digital Converter (ADC) are directly interconnected and can be configured to meet various application requirements. 

More information related to the modules interconnection you can refer to Motor Control application notes. AN13902, AN13884 or AN13767.

What advantages does LCU provides? LCU selects multiple inputs from timers, Pulse Width Modulation (PWM) signals, and Input/Output (I/O) pads, and combines them using a programmable logic function to create output waveforms.

 

BR, VaneB

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,121 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @anakha 

Do and why we need to route eMios PWM to LCU through TRGMUX? The Enhanced Modular IO Subsystem (eMIOS), Logic Control Unit (LCU), Trigger MUX (TRGMUX), Body Cross-triggering Unit (BCTU) and Analogue-to-Digital Converter (ADC) are directly interconnected and can be configured to meet various application requirements. 

More information related to the modules interconnection you can refer to Motor Control application notes. AN13902, AN13884 or AN13767.

What advantages does LCU provides? LCU selects multiple inputs from timers, Pulse Width Modulation (PWM) signals, and Input/Output (I/O) pads, and combines them using a programmable logic function to create output waveforms.

 

BR, VaneB

0 项奖励
回复
%3CLINGO-SUB%20id%3D%22lingo-sub-1896708%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%E4%B8%BA%E4%BB%80%E4%B9%88PWM%E8%A6%81%E7%94%A8LCU%EF%BC%9F%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1896708%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3E%E6%88%91%E4%BB%AC%E6%98%AF%E5%90%A6%E9%9C%80%E8%A6%81%E9%80%9A%E8%BF%87%20TRGMUX%20%E5%B0%86%20eMios%20PWM%20%E8%B7%AF%E7%94%B1%E5%88%B0%20LCU%EF%BC%9F%E4%B8%BA%E4%BB%80%E4%B9%88%EF%BC%9F%3C%2FP%3E%3CP%3ELCU%20%E6%9C%89%E5%93%AA%E4%BA%9B%E4%BC%98%E5%8A%BF%EF%BC%9F%3C%2FP%3E%3CBR%20%2F%3E%3CP%3E%E6%88%91%E6%AD%A3%E5%9C%A8%E4%BD%BF%E7%94%A8%E9%9D%9E%20autosar%20%E7%9A%84%20RTD%20(3.0.0)%E3%80%82%3C%2FP%3E%3C%2FLINGO-BODY%3E