What is the spatial ditribution of DFlash in S32K3?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the spatial ditribution of DFlash in S32K3?

ソリューションへジャンプ
1,808件の閲覧回数
jingfang
Contributor IV

We are going to user DFLASH instead of EEPROM in S32k3.

I want to know what is the minimum erasure space of DFLASH?Whether this area can be unlocked separately to protect data security?

0 件の賞賛
返信
1 解決策
1,802件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @jingfang,

The sector size is 8KB, and there is a lock for each of them.

You can start with the C40_Ip_Example_S32K144 RTD example.

And use the C40_Ip_ClearLock() function, where the first argument is C40_Ip_VirtualSectorsType VirtualSector.

In C40_Ip_Cfg.h you can find:

danielmartynek_0-1654777106491.png

 

Regards,

Daniel

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,649件の閲覧回数
ziomocci
Contributor IV

Hi All,

 we have to map all the flash memory (S32K3 f.y.i.) for different SW levels (Bootloader, Tunables, Main Application, NVM, etc etc) but there is something not totally clear for me.

According to the picture below

 

ziomocci_0-1663078102188.png

we have (8KB x 32) and (64KB x 12), for a total amount of 1MB of Flash for Block.

But what is the sector lock granularity for Block 4 Data Flash? 4 blocks of 32KB each one or 2 blocks of 64KB?

Regards,

Andrea

 

0 件の賞賛
返信
1,803件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @jingfang,

The sector size is 8KB, and there is a lock for each of them.

You can start with the C40_Ip_Example_S32K144 RTD example.

And use the C40_Ip_ClearLock() function, where the first argument is C40_Ip_VirtualSectorsType VirtualSector.

In C40_Ip_Cfg.h you can find:

danielmartynek_0-1654777106491.png

 

Regards,

Daniel

 

 

 

 

0 件の賞賛
返信