What is the scenario of data match wakeup/address wakeup/idle line wakeup in LPUART module?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the scenario of data match wakeup/address wakeup/idle line wakeup in LPUART module?

ソリューションへジャンプ
2,190件の閲覧回数
nathan_wang
Contributor I

I am using S32K1xx for LIN communication. I see data match wakeup/address wakeup/idle line wakeup of receiver features in S32K Reference Manual. So I wonder if these features are used in LIN communication? And what the scenario of these features?

タグ(2)
0 件の賞賛
返信
1 解決策
2,182件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@nathan_wang

    Idle line wakeup/Address mark wakeup/Receive data match can be used to wakeup MCU from STOP mode and can reduce ISR overhead.

Idle line wakeup:

      The receiver wakes up when detects a full character time of the idle-line level and generates an interrupt if enabled.

Address-mark wakeup

       The receiver wakes up when detects a logic 1 in the most significant bit of the received character/ when parity is enabled, the second most significant bit is used for address-mark wakeup, and generates an interrupt if enabled.

Data match wakeup

     The receiver wakes up when detects a character that matches MATCH[MA1] field when BAUD[MAEN1] is set, or that matches MATCH[MA2] when BAUD[MAEN2] is set, and generates an interrupt if enabled.

        Receiver wakeup and receiver address matching is a hardware mechanism that allows an
LPUART receiver to ignore the characters in a message intended for a different receiver.

        The S32K LPUART module has some of the features described above, but these features have nothing to do with LIN. The LIN standard does not require MCUs to have these features. The use of these features is entirely up to the user.

 

BR!

     Jim.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,183件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@nathan_wang

    Idle line wakeup/Address mark wakeup/Receive data match can be used to wakeup MCU from STOP mode and can reduce ISR overhead.

Idle line wakeup:

      The receiver wakes up when detects a full character time of the idle-line level and generates an interrupt if enabled.

Address-mark wakeup

       The receiver wakes up when detects a logic 1 in the most significant bit of the received character/ when parity is enabled, the second most significant bit is used for address-mark wakeup, and generates an interrupt if enabled.

Data match wakeup

     The receiver wakes up when detects a character that matches MATCH[MA1] field when BAUD[MAEN1] is set, or that matches MATCH[MA2] when BAUD[MAEN2] is set, and generates an interrupt if enabled.

        Receiver wakeup and receiver address matching is a hardware mechanism that allows an
LPUART receiver to ignore the characters in a message intended for a different receiver.

        The S32K LPUART module has some of the features described above, but these features have nothing to do with LIN. The LIN standard does not require MCUs to have these features. The use of these features is entirely up to the user.

 

BR!

     Jim.

0 件の賞賛
返信
2,163件の閲覧回数
nathan_wang
Contributor I

Hi@Senlent,

    Thanks for your reply. So are these features used in Infrared?

0 件の賞賛
返信
2,153件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@nathan_wang

       I may not understand what you mean, do you mean these features can be used for infrared?

       The scenarios in which these features are used are entirely up to the user。

BR!

0 件の賞賛
返信