What is right procedure to modify linker for bootloader in RTD3.0.0?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is right procedure to modify linker for bootloader in RTD3.0.0?

1,463件の閲覧回数
jerryrig
Contributor III

I am trying to update linker so that my application can be used with uds bootloader 2.0.0. However whenever i make changes in linker the application boot fails. My question here is what is right sequence / steps to modify linker for bootloader.

I have few question with linker and system MPU, what is purpose of following code, and how does it behave when application Address is modified,

 

system.c
.
.
.
    /* Program flash */
    rbar[14]=(uint32)((uint32)__ROM_CODE_START + 0x400000UL);
#if defined(S32K396) || defined(S32K394)
    rasr[14]=0x070B0029UL; /* Size: import information from linker symbol, Type: Normal, Inner Cache Policy: Inner write-back, write and read allocate, Outer Cache Policy: Outer write-back. write and read allocate, Shareable: No, Privileged Access: Read-Only, Unprivileged Access: Read-Only */
#elif defined(S32K358) || defined(S32K388) || defined(S32K328) || defined(S32K338) || defined(S32K348)
    rasr[14]=0x070B002BUL; /* Size: import information from linker symbol, Type: Normal, Inner Cache Policy: Inner write-back, write and read allocate, Outer Cache Policy: Outer write-back. write and read allocate, Shareable: No, Privileged Access: Read-Only, Unprivileged Access: Read-Only */
#else
    rasr[14]=0UL;
#endif
    

 

 

Why is int vector is moved from int_sram_no_cacheable in RTD2.0 to int_dtcm section in RTD3.0, does this need to be modified for bootloader?

 

    .int_vector :
    {
        . = ALIGN(2048);
        __interrupts_ram_start = .;
        . += __interrupts_init_end - __interrupts_init_start;
        . = ALIGN(4);
        __interrupts_ram_end = .;
    } > int_dtcm

 

 

Are there any migration steps for UDS on RTD3.0?

タグ(3)
2 返答(返信)

1,029件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @jerryrig 

There are demo applications available that showcase the usage of the Bootloader Jump to Application using RTD Version 3.0.0. I suggest reviewing these, as they are for a different device but could serve as a good starting point and reference for your application.

Example S32K312 Bootloader to Application Jump DS3.5 RTD300

Example S32K324 Bootloader to Application Jump DS3.5 RTD300

Additionally, for a better understanding of the MPU's register usage, please refer to the Arm Cortex-M7 documentation.

MPU Region Base Address Register

MPU Region Number Register

Could you also clarify the changes made to the origin address and size of the int_pflash?

 

BR, VaneB

0 件の賞賛
返信

1,459件の閲覧回数
jerryrig
Contributor III

This is screenshot of project after modifying flash address in linker in RTD3.0.0. I have also attached the linker file.

タグ(1)
0 件の賞賛
返信