What circumstances will cause the adc self-test algorithm return failure in S32K3xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What circumstances will cause the adc self-test algorithm return failure in S32K3xx

14,457 Views
Guo-
Contributor I

I am testing the ADC Self Test function on the S32K324 chip.

In order to test that the ADC can be detected when an error occurs, the ADC Reference high voltage is artificially set to zero on the hardware circuit to simulate ADC failure, but the ADC Self-Test algorithm still does not report an error (I use the AUTOSAR standard interface selftest API)

I confirmed that I removed the corresponding circuit because the ADC calibration did not pass and will enter dead loop.

I wonder what will cause the self test function failed and how I can test it.

B.R.

Guo

Tags (1)
0 Kudos
Reply
9 Replies

14,335 Views
Guo-
Contributor I

So in fact, in the autosar framework, the selftest api cannot detect whether the adc circuit outside the chip is working properly, but only whether the adc is working properly inside the chip. I think I got it. Thanks a lot.

0 Kudos
Reply

14,448 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I don't understand you whether you are setting VREFH to low during self-test or only during calibration. Anyway ADC self-test algorithm S tests reference voltage, so it should lead failed self-test results.

0 Kudos
Reply

14,428 Views
Guo-
Contributor I

I removed the VREFH circuit on the physical circuit. That means there is no input at this pin. Wheather that the VREFH needs to be grounded to make the self test error? I just simply disconnected VREFH pin. At the following image, I would like to show you how I start the self test after set the adc register to the correct value, and I hope it is helpful for you to find out why the self-test didn't work.

0 Kudos
Reply

13,499 Views
LeoZ
Contributor III
hi, are these code written by you manually, or from S32K Design Studio with some package?
0 Kudos
Reply

14,422 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is quite interesting, but it is possible that if you have VREFH unconnected, it may be evaluated as valid range due to induced voltage from other pins (not being completely sure). I would recommend you to try to terminate to GND.

14,412 Views
Guo-
Contributor I

Nope it still not work

I ground VREFH as you asked but self-test API still returns pass

To make the problem clearer, I would like to confirm to you whether I changed the circuit correctly: I ground the 16th pin of the MCU chip, other circuits do not change, I am using the S32K324 chip (S32K324  has 172 pins)

I would also like to know which error register would set 1 under “normal” circumstances? 

ADC_STSR1_ERR_S0 or ADC_STSR1_ERR_S1 or ADC_STSR1_ERR_S2?
0 Kudos
Reply

14,397 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I should fail is S0 as it converts band gap level according ADC reference.

0 Kudos
Reply

14,386 Views
Guo-
Contributor I

I still don't understand why self-test didn't work. After I turned on all the registers related to self-test as required by the chip reference manual, I could observe the repeated changes from 0 to 1 in the SELF_TEST_S (18bit) from MSR register by leaving the register in this state, which proves that selftest has started normally.

But the STSR1 register only has bit23 turned to 1(value: 0x00800000) which confirmed self-test end of conversion, I don't know after normal selftest ends, only bit23 in STSR1 will set 1 or the watch dog register should set to complete.

But according to your statement, bit11 in the STSR1 register, the Error Algorithm S step 0, will be set to 1 first?

I still need your help with this problem,I would like you to give me some ideas, or should I provide more clues?

0 Kudos
Reply

14,345 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have obtained an answer from SW developer, I am forwarding as it is:

"

The reason for the self-test executed successfully with VREFH tied to GND is that, the RTD Adc_Sar_Ip_SelfTest() only executes the self-test process but doesn't check the conversion data of each self-test algorithm step(such as S1), it means the error flag(such as STSR1[ERR_S1]) won't be set although the VREFH was tied to GND.

And the ADC also provides monitoring options for conversion data generated by self-test algorithms, for details, you could refer to "58.3.16.2.4 Self-test analog watchdog" in S32K3 RM.

1.png

To help the customer to complete this test, we need to enable the self-test analog watchdog and configure its low threshold value(15bit) which related to VERFH(self-test algorithm S1 and S2).

For example, I modified the RTD Adc_Sar_Ip_SelfTest() function by adding below code, then the self-test was failed because the conversion data(0x7DE0) of S1|S2 was less than the low threshold value which I configured(0x7FFF) before.

2.png

You could also find the conversion result when an error in step 1|2 of algorithm S has occurred as below.

3.png

 

 

 

"

0 Kudos
Reply