Voltage Drop on GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Voltage Drop on GPIO

2,456件の閲覧回数
hamid_abrishami
Contributor III

Hi every one!
we use S32K148 in our product. in data sheet it seems that said if we sink or source 5mA on typical GPIO or IohGPIO-HD_DSE_0 we have 0.8V drop on out put means: VoH(minimum) = 5 - 0.8 = 4.2 and VoL(Maximum) = 0 + 0.8 = 0.8
I want to know what happen if we source below this current for instance 4mA.
Dose we have any curve for illustrate the relation between the source current VS drop Voltage on output. 
what about GPIO-fast.

Thanks 


Screenshot 2022-12-20 114007.png

 

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,433件の閲覧回数
hamid_abrishami
Contributor III

thanks 
And what happen if we source current more than 5mA. Does Vout drop more than 0.8V ?  

0 件の賞賛
返信

2,431件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

As the source current becomes larger, the voltage drop will also become larger.

0 件の賞賛
返信

2,442件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

I want to know what happen if we source below this current for instance 4mA.

Then the actual output VoH is higher, that is, the voltage drop will not be as much as 0.8v.

Dose we have any curve for illustrate the relation between the source current VS drop Voltage on output. 

Sorry, I didn't find this kind of curve on the public information.

The following are the GPIO-FAST pins on the S32K148 chip:

GPIO-FAST Pad Type.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信