VR5510

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VR5510

2,520 次查看
zafeerferoz
Contributor I

Hi , 

We are developing a design based on S32K314 with VR5510 as the PMIC. There are two PWRON1 and ON2 pins mentioned in the document as Wake up. Can we use this pin only for the Wake up application. Mainly PWRON1 for an Ignition detect and PWRON2 for Wake up INH for the LIN or CAN. 

Regards

Zafeer

0 项奖励
回复
3 回复数

2,484 次查看
zafeerferoz
Contributor I

Hi Guofred, 

Thanks for the reply. Why we went with VR5510 is we have additional 3v8 @2A for a 4G module. 

Wrt to the PWRON1 and PWRON2 pins - In the below Table 81 - it is mentioned as these pin can be configured as Wake up event. Hope we can use like this

zafeerferoz_0-1671451426242.png

 

Regards

Zafeer

0 项奖励
回复

2,480 次查看
Guofred
Contributor III

Hi @zafeerferoz ,

Thanks for sharing the information, hope you goes well. 

yes, the hardware shows 2x input pin for wake-up detection.

may be we can check it again by using your development board. thanks.

Guofred_1-1671501872310.png.

 

Guofred_0-1671501334778.png

Best regards.

Guofred

 

0 项奖励
回复

2,511 次查看
Guofred
Contributor III

Hi @zafeerferoz 

1)  i think the NXP PMIC FS65/FS26 is more suitable for S32K3 

2)  about the VR5510 PWRON1 and PWRON2, the reference as below. thanks.  

Guofred_2-1671266469256.pngGuofred_3-1671266540118.png

Best regards.

Guofred

 

0 项奖励
回复