VR5510

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510

2,527 Views
zafeerferoz
Contributor I

Hi , 

We are developing a design based on S32K314 with VR5510 as the PMIC. There are two PWRON1 and ON2 pins mentioned in the document as Wake up. Can we use this pin only for the Wake up application. Mainly PWRON1 for an Ignition detect and PWRON2 for Wake up INH for the LIN or CAN. 

Regards

Zafeer

0 Kudos
Reply
3 Replies

2,491 Views
zafeerferoz
Contributor I

Hi Guofred, 

Thanks for the reply. Why we went with VR5510 is we have additional 3v8 @2A for a 4G module. 

Wrt to the PWRON1 and PWRON2 pins - In the below Table 81 - it is mentioned as these pin can be configured as Wake up event. Hope we can use like this

zafeerferoz_0-1671451426242.png

 

Regards

Zafeer

0 Kudos
Reply

2,487 Views
Guofred
Contributor III

Hi @zafeerferoz ,

Thanks for sharing the information, hope you goes well. 

yes, the hardware shows 2x input pin for wake-up detection.

may be we can check it again by using your development board. thanks.

Guofred_1-1671501872310.png.

 

Guofred_0-1671501334778.png

Best regards.

Guofred

 

0 Kudos
Reply

2,518 Views
Guofred
Contributor III

Hi @zafeerferoz 

1)  i think the NXP PMIC FS65/FS26 is more suitable for S32K3 

2)  about the VR5510 PWRON1 and PWRON2, the reference as below. thanks.  

Guofred_2-1671266469256.pngGuofred_3-1671266540118.png

Best regards.

Guofred

 

0 Kudos
Reply