VLPS differences S32K144 and S32K146 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VLPS differences S32K144 and S32K146 ?

2,739件の閲覧回数
stabilo
Contributor II

Dear support team,

Are there some differences between the S32K144 and S32K146 very low power mode (VLPS) ?

I use this sequence to go to very low power mode:

During the initialization:

  • I set SMC_PMPROT_AVLP to 1
  • I set SMC_PMCTRL_STOPM to 2
  • I set SMC_STOPCTRL_STOPO to 0
  • I set SCB_SCR_SLEEPDEEP to 1

When I want to to go very low power mode:

  • I switch off the unused peripherals (PCC registers)
  • I start my wake up timer (LPTMR)
  • I execute the WFI instruction

With my hardware with S32K146, the current consumption in sleep mode is 5mA higher than with the other hardware (with S32K144).

is this normal that the S32K146 consumes 5mA more than the S32K144 (in VLPS or RUN mode) ?

Thank you very much

0 件の賞賛
返信
1 返信

2,255件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,
As per S32K1xx Datasheet, the consumption in VLPS of S32K146 is slightly higher (+20uA, Table 7 of DS) than the consumption of S32K144.
5mA is really too much.
The board must run stand-alone without debugger to enter VLPS.
Can you check VLPSA bit? Do you drive any external load?

Regards,
Daniel

0 件の賞賛
返信