PWM configuration at Hz [S32K144]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM configuration at Hz [S32K144]

Jump to solution
2,876 Views
electronica2pow
Contributor III

Hi to the community,

I am trying  to configure a PWM output between 300 and 600 Hz (FTM0, channel 0), in order to get this goal i must introduce the higher possible number on MOD(16 bits) register to reduce frequency, but its maximum available value is 65535(2^16 - 1), reaching a frequency around 1 KHz.

Is it possible on S32K144 to get those frequencies?

I am using this code: 

void Edge_Align_PWM_Init() {

/* Enable clock for PORTD */

PCC->PCCn[PCC_PORTD_INDEX] = PCC_PCCn_CGC_MASK;

/* Select and enable clock for FTM0 */

PCC->PCCn[PCC_FLEXTMR0_INDEX] = PCC_PCCn_PCS(6) | PCC_PCCn_CGC_MASK;

/* Set PORTD pins for FTM0 */

PORTD->PCR[15] = PORT_PCR_MUX(2); // FTM0, Channel0 

PORTD->PCR[16] = PORT_PCR_MUX(2); // FTM0, Channel1

PORTD->PCR[0] = PORT_PCR_MUX(2); // FTM0, Channel2

PORTD->PCR[1] = PORT_PCR_MUX(2); // FTM0, Channel3

/* Enable registers updating from write buffers */

FTM0->MODE = FTM_MODE_FTMEN_MASK;

/* Enable sync, combine mode and dead-time for pair channel n=1 and n=2 */

FTM0->COMBINE = 0x0u | FTM_COMBINE_COMP1_MASK | FTM_COMBINE_DTEN1_MASK;

/* Set Modulo in initialization stage (10kHz PWM frequency @112MHz system clock) */

FTM0->MOD = FTM_MOD_MOD(64000-1);//11200->10KHz

/* Set CNTIN in initialization stage */

FTM0->CNTIN = FTM_CNTIN_INIT(0);

/* Enable high-true pulses of PWM signals */

FTM0->CONTROLS[0].CnSC = FTM_CnSC_MSB_MASK | FTM_CnSC_ELSB_MASK;

FTM0->CONTROLS[1].CnSC = FTM_CnSC_MSB_MASK | FTM_CnSC_ELSB_MASK;

/* Set channel value in initialization stage */

FTM0->CONTROLS[0].CnV=FTM_CnV_VAL(32000); // 50% duty cycle 

FTM0->CONTROLS[1].CnV=FTM_CnV_VAL(32000); // 50% duty cycle 

/* Reset FTM counter */

FTM0->CNT = 0;

/* Insert deadtime (1us) */

FTM0->DEADTIME = FTM_DEADTIME_DTPS(3) | FTM_DEADTIME_DTVAL(7);// 3 y 7

/* Clock selection and enabling PWM generation */

FTM0->SC = FTM_SC_CLKS(1) | FTM_SC_PWMEN0_MASK | FTM_SC_PWMEN1_MASK | FTM_SC_PWMEN2_MASK | FTM_SC_PWMEN3_MASK;

}

Best regards,

Jorge

Tags (2)
1 Solution
2,036 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jorge,

Do you need to use SPLLDIV1_CLK as FTM functional clock?
Using SOSCDIV1_CLK you can get much lower frequency.
PCC->PCCn[PCC_FLEXTMR0_INDEX] = PCC_PCCn_PCS(1) | PCC_PCCn_CGC_MASK;

Also, you can prescale the frequency in FTMn_CS[PS] register.

Regards,
Daniel

View solution in original post

2 Replies
2,037 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jorge,

Do you need to use SPLLDIV1_CLK as FTM functional clock?
Using SOSCDIV1_CLK you can get much lower frequency.
PCC->PCCn[PCC_FLEXTMR0_INDEX] = PCC_PCCn_PCS(1) | PCC_PCCn_CGC_MASK;

Also, you can prescale the frequency in FTMn_CS[PS] register.

Regards,
Daniel

2,036 Views
electronica2pow
Contributor III

I chose to modify the PS register.

Thanks Daniel!

0 Kudos