VLPS &LPIT & CAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

VLPS &LPIT & CAN

2,234 次查看
panda_fei
Contributor II

What is the difference between debug and run mode?

Why does lpit wake up s32k144 running in VLPs mode in debug mode?

为什么仅仅初始化了CAN模块,CAN可以唤醒S32K在VLPS模式?

Why CAN can wake up S32K in VLPS mode,just initialize the CAN module ?

thank you very much

0 项奖励
回复
1 回复

1,907 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

As you can see in Chapter 53.13 Debug in low-power modes, with debug enabled, transitions from Run directly to VLPS are not allowed and result in the system entering Stop mode instead.

So, in this case, it seems the LPIT wake up from VLPS.

But in stand-alone mode the LPIT as well as CAN cannot wake up from VLPS.

 

Regards,

Daniel

0 项奖励
回复