VLPS &LPIT & CAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VLPS &LPIT & CAN

2,300件の閲覧回数
panda_fei
Contributor II

What is the difference between debug and run mode?

Why does lpit wake up s32k144 running in VLPs mode in debug mode?

为什么仅仅初始化了CAN模块,CAN可以唤醒S32K在VLPS模式?

Why CAN can wake up S32K in VLPS mode,just initialize the CAN module ?

thank you very much

0 件の賞賛
返信
1 返信

1,973件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

As you can see in Chapter 53.13 Debug in low-power modes, with debug enabled, transitions from Run directly to VLPS are not allowed and result in the system entering Stop mode instead.

So, in this case, it seems the LPIT wake up from VLPS.

But in stand-alone mode the LPIT as well as CAN cannot wake up from VLPS.

 

Regards,

Daniel

0 件の賞賛
返信