my client made a S32K344 board ,the V15 is power by a BJT , but the voltage for V15 is about 0.2V while the PET13 is 0 voltage.
i checked the EVK the V15 is about 0.1V and the PET13 is 0 voltage.
can anyone help me ?
解決済! 解決策の投稿を見る。
i found the power_1 module in which one can config the regulater.
元の投稿で解決策を見る
Hi @steven_zhang,
Is the LMBCTLEN bit set?
Please refer to Figure 159. Last-mile regulator enable sequence in the RM, rev.4
BR, Daniel