Using SENT as Triggered SENT using Flex IO peripheral

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using SENT as Triggered SENT using Flex IO peripheral

1,318 Views
AVargh23
Contributor III

Can a FlexIO pin be used as an output to send trigger and then receive SENT frames for S32K344? The example project has it set up for FlexIo Sent Receiver alone. Is it possible to make use of the same to act as an output to send trigger pulses to SENT device  and then change it to input to receive the SENT frames? 

Tags (3)
0 Kudos
Reply
1 Reply

1,293 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it is apparently not possible to do it with FlexIO. Pay attention to following thread:
https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-FlexIO-configuration-to-SENT-SAE-J2...

 

0 Kudos
Reply