Hello @Yash2530 ,
I performed a reference test using an S32K3X8EVB-Q289 and the on-board PEmicro debugger connected through J55.
In my test, the first CRC verification also reported a mismatch because the existing flash content was different from the application being downloaded. However, the programming sequence then continued with flash erase and programming. Therefore, the initial CRC mismatch is not necessarily the root cause and does not, by itself, confirm that Secure Debug is enabled.
The important difference is that, in the log you provided, the debug session terminates immediately after the first VC command. I do not see the subsequent EM and PM commands for erasing and programming the flash.
Please check the PEmicro debug launch configuration, particularly whether downloading the executable and flash programming are enabled. Please also provide the complete PEmicro log from the beginning of the session. The beginning of the log should show the CM command and the selected .arp flash algorithm.
For reference, my successful test used the following algorithm for an HSE-disabled device:

Please verify that the algorithm selected in your configuration corresponds to the actual state of your S32K358 device, for example HSE-disabled or HSE-enabled.
BTW, please create a new thread next time - we actively tracked community threads only 7 days after last answer. I only receive subscription emails for updates and those can occasionally be missed.
Best regards,
Pavel