Using S32K312 FEE module to write dataflash values is incorrect.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using S32K312 FEE module to write dataflash values is incorrect.

Jump to solution
1,821 Views
victory
Contributor V

Dear NXP,

1.When the code sets to write DataBlock0[4] = {0x55,0x55,0x55,0x55}, it is found that the value of dataflash does not match DataBlock0[4], as shown in the following figure.

victory_0-1719403395219.png

2.Detailed code, as attached.

I hope for your timely reply, thank you.

Regards,

YouSheng Liu

0 Kudos
Reply
1 Solution
1,748 Views
victory
Contributor V

The problem has been solved.

 

Thank you,

View solution in original post

0 Kudos
Reply
2 Replies
1,792 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @victory,

What RTD 4.0.0 version do you use?

I see many errors reported by the configuration tool in AUTOSAR 4.4 Version 4.0.0 P24.

Can you send a functional compiled test project so that I can test it?

 

Thank you,

Daniel

0 Kudos
Reply
1,749 Views
victory
Contributor V

The problem has been solved.

 

Thank you,

0 Kudos
Reply