Unlock s32k144 timeout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unlock s32k144 timeout

ソリューションへジャンプ
3,150件の閲覧回数
Ivan6
Contributor II

Hi,

 
I try to modify the program start address in keil5 . when debug the program by jlink, the mcu cannot connect. I uesd another mcu is same. 
    Form community,I try to connect swd inrest pin to gnd, "unlock kinetis" always timeout.
How to fix ,thanks.
 
Ivan6_0-1651202647282.png

 J-link commander 

Ivan6_1-1651202775682.png

 

Ivan6_2-1651202884895.png

 

0 件の賞賛
返信
1 解決策
3,140件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@lvan6

please refer to fellowing document.

S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解 

The flash configuration field is a 16-byte section of flash memory located at 0x400-0x40F.

The cause of the chip lockup may be that you wrongly modified the link file

Senlent_0-1651220746367.png

If the user disables mass erase with no other means to unsecure the device (no backdoor
key and no firmware means of changing the default security options), then that device
will be permanently secured.

BR!

      Jim,

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,141件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@lvan6

please refer to fellowing document.

S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解 

The flash configuration field is a 16-byte section of flash memory located at 0x400-0x40F.

The cause of the chip lockup may be that you wrongly modified the link file

Senlent_0-1651220746367.png

If the user disables mass erase with no other means to unsecure the device (no backdoor
key and no firmware means of changing the default security options), then that device
will be permanently secured.

BR!

      Jim,

 

0 件の賞賛
返信