Unhandled Exception Occurs after compiling SCST library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unhandled Exception Occurs after compiling SCST library

2,197件の閲覧回数
surya_phaniteja
Contributor II

Hi,

We are trying to integrate the SCST lib (SCST_M4_S32K144_RTM_1.0.5) in our project which run on the S32K148 controller with the compiler GHS

I am able to successfully compile all the assembly files (44). But during execution, the control struck at "Unhandled exception" which is further leading to the "HAL_CORE_FREEZE" and the control struck at this point continuously. Please find below image

I have observed if i am going to build individual assembly files (only one at a time), then the execution was proper without getting unhandled exception.

Can someone please suggest me how can i avoid unhandled exception here?

Thanks,

Surya

 

0 件の賞賛
返信
0 返答(返信)