Hello @durga_choudhury,
S32DS Config Tools share functionality between other families (such as S32Z, S32N, S32G, etc.). You can see that when selecting a S32K MCU, SERDES Serializer/Deserializer tool (along with DCD, IVT, QuadSPI, DDR, among others) are disabled, since it is not supported:

Same reason for enable_parallel_routing configuration. You can enable/disable this from "Project > Properties > S32 Configuration Tools > Enable Parallel Routing", and it is shared between families using Pins tool.

Even though I was not able to find within the documentation a description for this, when enabled, the Pins tool will prompt the user during signal routing if another signal shares the same physical pin and writes to the same PORT register with the same configuration values.
The tool will ask whether to automatically co-route all such signals simultaneously. I can reproduce this by configuring WKPU signal sharing configuration values with ADC in S32K3:

If disabled, this prompt is not present.
Best regards,
Julián