Unable to using MSD flash programmer for S32K118EVB2Q48

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to using MSD flash programmer for S32K118EVB2Q48

Jump to solution
3,682 Views
Zomebies
Contributor I

Dear Sirs,

I would like to use MDS flash programmer to program new flash image. I build the hello_world_s32K118 and get the hello_world_s32k118.srec image. When I copy the image to the drive with
a volume label of S32K118EVB, the led in EVB.  is 2s off followed by 8 rapid on/off blinks, the state "error 7" in LASTSTAT.TXT file. However, I could use S32DS debugger(SWD) to program the same hello_world example successfully. S
o could anyone give any suggestion for this issue? Thanks!

My Environment is,

EVAL Board : S32K118EVB2Q048

OS : WIN10 21H1

S32 Design Studio for S32 Platform Version: 3.4

SDA_INFO.HTM :

Zomebies_1-1638928473655.png

 

0 Kudos
Reply
1 Solution
3,649 Views
Zomebies
Contributor I

Hi, Robin,

Thanks for your suggestion. I got the root cause for MSD programming. The lastest MSD-DEBUG-S32K118EVB-Q064_Pemicro_v123.SDA is compatible with S32K118EVB-Q048.

View solution in original post

0 Kudos
Reply
2 Replies
3,668 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

The latest OpenSDA Firmware from PEMicro is for S32K118EVB-Q064: (Pemicro_OpenSDA_Debug_MSD_Update_Apps_2020_05_12\MSD-DEBUG-S32K118EVB-Q064_Pemicro_v123.SDA)

I am not sure if there is a firmware corresponding to S32K118EVB2Q048.
It is recommended that you submit a Support Requests to PEMicro and ask them if the problem is caused by a mismatch in firmware application.

The LED Status Indicator it's: 

LED Status Indicator.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,650 Views
Zomebies
Contributor I

Hi, Robin,

Thanks for your suggestion. I got the root cause for MSD programming. The lastest MSD-DEBUG-S32K118EVB-Q064_Pemicro_v123.SDA is compatible with S32K118EVB-Q048.

0 Kudos
Reply