Unable to use round function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to use round function

ソリューションへジャンプ
2,870件の閲覧回数
DemaQasem
Contributor II

Hello,

I am implementing a project on S32K144 using the S32DS IDE v3.4, when I use the "round" function and build the project I get the error  : 

DemaQasem_0-1707044718193.png

 

even though I made sure to include the math.h library
any reason for that  ?

Thank you.

タグ(2)
0 件の賞賛
返信
1 解決策
2,841件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

math.h is only header file for math library. You need to add libm.a library into your project in project properties: 

jiri_kral_0-1707130775057.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,842件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

math.h is only header file for math library. You need to add libm.a library into your project in project properties: 

jiri_kral_0-1707130775057.png

 

0 件の賞賛
返信
2,163件の閲覧回数
rithic
Contributor II

Is there a similar solution for the imxrt1176 

I am getting a similar error this is the embedded coder window

rithic_0-1737554784335.png

 

The exact error from the diagnostic window

rithic_1-1737554842734.png

 

 

0 件の賞賛
返信
2,158件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I'm not familiar with imxrt1176 and it's development tool, but the principle is very same. You need add math library and let the linker know where the library archive is (library path - if it is not already configured). 

0 件の賞賛
返信
2,808件の閲覧回数
DemaQasem
Contributor II
thank you so much ! it worked.
0 件の賞賛
返信