Two CS in SPI0 line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Two CS in SPI0 line

965件の閲覧回数
manojkumar_123
Contributor II

Hi,

am using "FS32K148UJT0VLUT" and wanted to connect Two ADC's for SPI0 with different CS. SPI0_CS1, SPI0_CS0. Does it work?

タグ(3)
0 件の賞賛
返信
1 返信

948件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Do you want to select a different salve via SPI0_CSx? Yes, you can select different slaves through SPI0_CS0~SPI0_CS3.

Multiple slave devices are selected using individual slave select (SS) lines.pngMultiple slave devices are selected using individual slave select (SS) lines.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信