Tresos missing mandatory module

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Tresos missing mandatory module

2,158件の閲覧回数
Jasmin_IM
Contributor III

Hi,

I always get the warning 11115 in Tresos that the Resource module is missing:

2025-02-21_075516.jpg

 

Project: esc_app<br>Missing mandatory module "Resource_TS_T40D34M30I0R0" in project "esc_app": Please add the module to the Module Configurations.

I have the 5.0.0 version installed. So, why is it still complaining about the old one?

2025-02-21_075711.jpg

It has no impact on functionality, it is just annoying. Is it perhaps an EB Tresos issue?

I searched for the Resource_TS_T40D34M30I0R0 string and cannot find it anywhere, except in the ".tresoslog" file.

0 件の賞賛
返信
3 返答(返信)

2,132件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Jasmin_IM,

I'm not sure if this is an issue on EB Tresos or our RTD SW. It may be an issue regarding multiple versions inside the plugins folder.

Do you have multiple versions for the RTD installed?

Let me ask the team internally to see what causes this issue.

Best regards,
Julián

0 件の賞賛
返信

2,045件の閲覧回数
Jasmin_IM
Contributor III

Hi Julián,

yes, I have:

 

2025-03-03_080037.jpg

(ignore that in this screenshot version 3 is used and not 5, it is a different branch state currently). 

This different version shouldn't matter. For every other component also 3 different versions are shown, only one is selected, and no component is reporting a warning, except "Resource".

Any news from the internal team?

Kind regards,
Jasmin

0 件の賞賛
返信

2,029件の閲覧回数
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Jasmin_IM,

Not yet, I imagine it will take some time to track/test the issue, as this does not affect functionality for code generation or loading modules.

I will update you if there is a response from the team.

Best regards,
Julián