Hi KKumar,
According to the description in "47.4.3.6 Channel (n) Value (C0V - C7V)" of S32K1xx MCU Family - Reference Manual, CnV should be wrote when the channel in output mode. But according to your codes and "Table 47-5. Channel Modes Selection", seems that channel 0 is not configured as output mode. So during debug you may find that the FTM0_C0V is always 0.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------