There is no version 3.5 of s32 design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There is no version 3.5 of s32 design studio

208 Views
hs41lee
Contributor I

Hello,
I need s32 design studio 3.5, but when I search, versions 3.6 and 3.4 appear clearly, while version 3.5 does not appear in my account.
It does appear in another person's account.
What should I do?

0 Kudos
Reply
1 Reply

174 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Only users who previously had access to S32DS 3.5 will still see it available.
New users will no longer see S32DS 3.5 automatically.
If needed, here is the download link for S32DS 3.5: https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32DS-3-5

By the way, why doesn't the customer use the latest S32DSv3.6.6?
I saw the following information in the "S32 Design Studio 3.6.0 Release Announcement":
Development, Add-Ons and Extension Packages delivered with older S32Design Studio 3.5.x are compatible with version 3.6.0
RTD and Runtime Software releases made on top of S32Design Studio 3.5.x are backward compatible with S32Design Studio 3.6.0 using smart compatibility mechanism


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

0 Kudos
Reply