There happen some error When I use S32 DS open WDOG_Example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There happen some error When I use S32 DS open WDOG_Example

2,489 Views
_simple_
Contributor III

I  use S32 Design Studio for ARM Version: 1.3  Build id: 170119,There happen some error When I use S32 DS open WDOG_Example? No such file or directory main.c /WDOG_Example/Sources line 60 C/C++ Problem,Who can help me solve this problem? 

Thanks!

 

 

177807_177807.PNG捕获.PNG

177808_177808.PNG捕获2.PNG

Labels (1)
0 Kudos
Reply
4 Replies

2,326 Views
raresvasile
NXP Employee
NXP Employee

Hi,

It seems that PEx code was not generated. Please try to generate the configuration structures and file links by clicking on Project -> Generate Processor Expert Code. 

pastedImage_2.png

Best regards,

Rares

0 Kudos
Reply

2,326 Views
_simple_
Contributor III

Thanks,According to what you said, I try it, But the problem still exists.

Thanks for your help

0 Kudos
Reply

2,326 Views
raresvasile
NXP Employee
NXP Employee

What version of the SDK are you using?

Can you attach the project?

Thanks

0 Kudos
Reply

2,326 Views
_simple_
Contributor III

The SDK version is S32 Design Studio for ARM Version: 1.3

File->Import->S32DS Example Project

捕获.PNG

捕获2.PNG

0 Kudos
Reply