The defined global macro is not recognized

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The defined global macro is not recognized

1,062件の閲覧回数
Elaina
Contributor I

I have a project in which a macro "RBD_PK_MINI" is defined in the "properties->C/C++ General->Paths and Symbols" of the project, but the piece of symbols in the code is gray, and the jump of "Ctrk+cliked" cannot be realized.I don't seem to have a definition, but I've defined it.This is a project imported from somewhere else.

Annotation 2024-04-22 145630.png

Annotation 2024-04-22 145728.png

This problem does not appear on my other computer, but it is the same project, I did not change it, I hope to get help, thank!

Best Regards

Elaina

0 件の賞賛
返信
1 返信

984件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Elaina, 

try to create new workspace and import your project into it. 

0 件の賞賛
返信